Command: CSV Export of Alarm Storage Permalink

Function: The command opens the “Alarm Storage Export Configuration” dialog.

Call: Context menu of the “Alarm Storage” object.

Requirements: The application is in online mode with an alarm configuration. An alarm storage is configured.

The command opens the “Alarm Storage Export Configuration” dialog.

Dialog: Alarm Storage Export Configuration – Basic Settings

“Export file”: Path to the generated CSV file in the file system

Table 804: Alarms to be exported

“Export all”

All listed alarms are exported.

“Export alarms in timestamp range (timestamp activated)”

Defined time range for the export of the listed alarms. This refers to the time stamp when the alarm was activated. The min./max. time stamps that are available in the alarm storage or were the last ones to be used in an export are shown by means of "From" and Until".

When selecting the time range, the smallest unit is one second.

Table 805: Language

“Language”

The list box includes all languages that are available in text lists for alarm texts, as well as the default language (<standard>).

Dialog: Alarm Storage Export Configuration – Advanced Settings

Table 806: Sorting by time stamp enabled

“Ascending”

“Descending”

Sort order by the time stamp when the alarm was activated

Table 807: File format

“Formatted values and timestamps”

The time stamps are formatted with the date and time format as defined below. ‎REAL‎ and ‎LREAL‎ values are formatted in number format.

“Raw data from alarm storage file”

The time stamps and values are written unformatted to the CSV file, as they appear in the alarm storage. Alarms, alarm groups, and alarm classes are written in non-readable form to the CSV file as internal IDs.

Table 808: Formatting options

Defines the formatting of the entries in the CSV file. Possible only if the “Formatted values and timestamps” data format is selected.

“REAL format (printf syntax)”

Setting: “%.1f”

“Date format”

The settings are applied from the system control.

“Time format”

The settings are applied from the system control.

Table 809: Separator

“Semicolon”

The entries in the CSV file are separated by a semicolon.

“Comma”

The entries in the CSV file are separated by a comma.

“Tab”

The entries in the CSV file are separated by a tab.

“Local time”

Available only if the “Formatted values and timestamps” data format is selected.

_cds_icon_option_activated_copy.png: The time stamps are written to the CSV file in local time.

_cds_icon_option_deactivated.png: The time stamps are written to the CSV file in universal time coordinated (UTC).